MTRCKTSPNSVM128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MTRCKTSPNSVM128

1,091 Views
lin_li
Contributor I

excuse me, why the MTRCKSPNZVM128: 3-phase Sensorless PMSM Development Kit include a BLDC instead of PMSM?

Is it a PMSM Development Kit?

0 Kudos
Reply
1 Reply

978 Views
RadekS
NXP Employee
NXP Employee

Hi Lin,

I just checked old threads and I see that your question is not answered.

I am sorry for out late response, we somehow missed it.

 

Yes, MTRCKSPNZVM128 is PMSM Development Kit.

In fact, the board and motor in MTRCKTSBNZVM128 (BLDC) and MTRCKTSPNZVM128 kits are the same.

The difference is in different jumper settings and mainly in software.

 

The Linix motor is officially BLDC type, but the motor characteristics are rather close to PMSM type.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply