MTRCKTSPNSVM128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MTRCKTSPNSVM128

1,088 次查看
lin_li
Contributor I

excuse me, why the MTRCKSPNZVM128: 3-phase Sensorless PMSM Development Kit include a BLDC instead of PMSM?

Is it a PMSM Development Kit?

0 项奖励
回复
1 回复

975 次查看
RadekS
NXP Employee
NXP Employee

Hi Lin,

I just checked old threads and I see that your question is not answered.

I am sorry for out late response, we somehow missed it.

 

Yes, MTRCKSPNZVM128 is PMSM Development Kit.

In fact, the board and motor in MTRCKTSBNZVM128 (BLDC) and MTRCKTSPNZVM128 kits are the same.

The difference is in different jumper settings and mainly in software.

 

The Linix motor is officially BLDC type, but the motor characteristics are rather close to PMSM type.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复