MTRCKTSPNSVM128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MTRCKTSPNSVM128

1,122件の閲覧回数
lin_li
Contributor I

excuse me, why the MTRCKSPNZVM128: 3-phase Sensorless PMSM Development Kit include a BLDC instead of PMSM?

Is it a PMSM Development Kit?

0 件の賞賛
返信
1 返信

1,009件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Lin,

I just checked old threads and I see that your question is not answered.

I am sorry for out late response, we somehow missed it.

 

Yes, MTRCKSPNZVM128 is PMSM Development Kit.

In fact, the board and motor in MTRCKTSBNZVM128 (BLDC) and MTRCKTSPNZVM128 kits are the same.

The difference is in different jumper settings and mainly in software.

 

The Linix motor is officially BLDC type, but the motor characteristics are rather close to PMSM type.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信