MSCAN on MC9S12C32 micro

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSCAN on MC9S12C32 micro

3,278 Views
CANproject
Contributor I
Hi
 
Does anybody have some knowledge  about the MSCAN module and the communication between two MC9S12C32 microcontrollers? I´m already using the AN3034SW example and is runnig good with some changes that I made to the code to fit on my micro, but I don´t know how to communicate two micros I just run the code in loop back mode, Please help me if you have some ideas for this. Thanks 
Labels (1)
0 Kudos
Reply
3 Replies

1,638 Views
Lundin
Senior Contributor IV
I assume that you have the proper hardware between the two MCU:s? That is, CAN tranceivers and bus termination. Apart from that, it shouldn't be different from loopback mode.
0 Kudos
Reply

1,638 Views
CANproject
Contributor I

HI

 

Thanks for the response. No I’m not using any transceiver & bus terminator, do you have some recommendations of any kind of transceiver & bus termination that I could use on my, project? Because with the loop back mode I just run the program and it seems to work great, but for my testing I need to build the bus between the two micros. Please let me know anything else that you could help me about this matter.

 

Thanks.

0 Kudos
Reply

1,638 Views
Lundin
Senior Contributor IV
I'm using MCP2551 myself (assuming you are using high-speed CAN) which is good when it comes to transient voltages and EMC. Since the pinout is standard it doesn't really matter which one you pick.

Bus termination of 120 ohm is CAN standard.
0 Kudos
Reply