MM9Z1J638 msCAN cant exit the initialization mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1J638 msCAN cant exit the initialization mode

ソリューションへジャンプ
1,878件の閲覧回数
Lin_Siul2u
Contributor I

Hi:

I encountered some issues when using the MsCAN of MM9Z1J638. I found that when I called the Init_CAN function for initialization, the return value would return ERR_INIT. After checking the specific content of the Init_CAN function, I discovered that after entering the initialization mode (INITAK == 1 && INITRQ == 1), when I completed the initialization configuration and attempted to exit the initialization mode by writing 0 to CANCTL0.INITRQ, I found that the INITAK value was still equal to 1. That is, the initialization did not exit. Could you please tell me what might be the possible reasons for this situation?

#MM9Z1638 #msCAN

0 件の賞賛
返信
1 解決策
1,867件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Lin_Siul2u,

What clock source have you selected in CANCTL1[CLKSRC]?

If you use the Oscillator clock, is the clock enabled?

 

Thank you,

BR, Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,868件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Lin_Siul2u,

What clock source have you selected in CANCTL1[CLKSRC]?

If you use the Oscillator clock, is the clock enabled?

 

Thank you,

BR, Daniel

0 件の賞賛
返信
1,874件の閲覧回数
Lin_Siul2u
Contributor I

btw,i am using the CAN0,and the reset mode is set as FAST.

0 件の賞賛
返信