MM9Z1J638 Current calibration problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1J638 Current calibration problem

3,124件の閲覧回数
cui1
Contributor II

According to the current calibration configuration on the AN12301, I found that the maximum test current was only ±50A.

cui1_0-1706004310897.png

cui1_1-1706004322843.png

cui1_2-1706004332720.png

 

 

0 件の賞賛
返信
5 返答(返信)

3,099件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello cui1,

I hope all is great with you. Thank you for using the NXP communities.

Could you please share further details about the HW used? I mean, are you using a custom board or an NXP evaluation board?

Regards,

David

3,095件の閲覧回数
cui1
Contributor II
Hello David,
I used the NXP evaluation board,The hardware interfaces refer to the official ones.
Regards,
cui
0 件の賞賛
返信

3,078件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello cui1,

Could you please confirm that VSENSE and TSENSE are disabled? Is the chopper enabled?

Regards,

David 

3,053件の閲覧回数
cui1
Contributor II
Hello David,
The above program follows the NXP software template, non-calibration module, normal reading current can reach 700A, calibration module program, reading current can only reach the maximum 50A
Regards,
Cui1
0 件の賞賛
返信

3,061件の閲覧回数
cui1
Contributor II
Hello David,
As shown above, the voltage and temperature are disabled and the current is activated. I think it has something to do with gain, please refer to it.
Regards,
Cui1
0 件の賞賛
返信