MM9Z1J638 Current calibration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1J638 Current calibration problem

3,099 Views
cui1
Contributor II

According to the current calibration configuration on the AN12301, I found that the maximum test current was only ±50A.

cui1_0-1706004310897.png

cui1_1-1706004322843.png

cui1_2-1706004332720.png

 

 

0 Kudos
Reply
5 Replies

3,074 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello cui1,

I hope all is great with you. Thank you for using the NXP communities.

Could you please share further details about the HW used? I mean, are you using a custom board or an NXP evaluation board?

Regards,

David

3,070 Views
cui1
Contributor II
Hello David,
I used the NXP evaluation board,The hardware interfaces refer to the official ones.
Regards,
cui
0 Kudos
Reply

3,053 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello cui1,

Could you please confirm that VSENSE and TSENSE are disabled? Is the chopper enabled?

Regards,

David 

3,028 Views
cui1
Contributor II
Hello David,
The above program follows the NXP software template, non-calibration module, normal reading current can reach 700A, calibration module program, reading current can only reach the maximum 50A
Regards,
Cui1
0 Kudos
Reply

3,036 Views
cui1
Contributor II
Hello David,
As shown above, the voltage and temperature are disabled and the current is activated. I think it has something to do with gain, please refer to it.
Regards,
Cui1
0 Kudos
Reply