MM9Z1_638 Power consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1_638 Power consumption

Jump to solution
3,054 Views
Boris_Bloxsberg
Contributor III

Hi there,

 

I´m using a MM9Z1_938 and I need to reduce the power consumption because I want to reduce the self heating of the IC. Is there a possibly or configuration to reduce the power consumption of the IC?

 

Regards

0 Kudos
Reply
1 Solution
2,983 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Boris_Bloxsberg,

Using the lower-power modes of the device.

Disabling unused peripherals:

danielmartynek_0-1637053944845.png

Make sure no inputs are floating, especially in the low-power modes.

 

Regards,

Daniel

View solution in original post

3 Replies
3,041 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Boris,

The power consumption is proportional to the system clock frequency.

You need to reduce the frequency as much as possible for this application.

 

BR, Daniel

2,992 Views
Boris_Bloxsberg
Contributor III

Hi,

 

thanks for the reply. The clock frequency way is working.

Are there any other ways aviable?

 

regards

0 Kudos
Reply
2,984 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Boris_Bloxsberg,

Using the lower-power modes of the device.

Disabling unused peripherals:

danielmartynek_0-1637053944845.png

Make sure no inputs are floating, especially in the low-power modes.

 

Regards,

Daniel