MM9Z1_638 Filter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,866件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

some weeks ago I added a question regarding the Filter of the MagniV.

Now, I´ve got an additional question....

At page 139 of the manual of the MM9Z1_638  I found the main structure of the implemented low pass filter. In table 192, I found the value conversation: "Data Format: MSB = Sign (“1” minus)"

Does it mean, you are using the twos complement? and is there an excel sheet aviable to calculate new values?

regards.

0 件の賞賛
返信
1 解決策
2,853件の閲覧回数
StanoA
NXP TechSupport
NXP TechSupport

Hi Boris,

It is used the fractional arithmetic in this case so the MSB is sign bit. The number is in range of +-1.000 on 15-bits (14:0).

Attached is the excel sheet for this calculation too.

I hope it could help you in your task.

Best Regards,

Stano.

元の投稿で解決策を見る

1 返信
2,854件の閲覧回数
StanoA
NXP TechSupport
NXP TechSupport

Hi Boris,

It is used the fractional arithmetic in this case so the MSB is sign bit. The number is in range of +-1.000 on 15-bits (14:0).

Attached is the excel sheet for this calculation too.

I hope it could help you in your task.

Best Regards,

Stano.