MM912J637 Vref Setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM912J637 Vref Setting

ソリューションへジャンプ
1,716件の閲覧回数
mrunaljoshi
Contributor II

Hi!

I am working on MM912J637 iBS. How can i change Vref for the  inbuilt adc ? I am not able to find  a specific vref setting in the datasheet. Can someone please suggest a solution?

Thanks . 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,623件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

looking at the datasheet it seems like it is not possible to change Vref.

In the Current and Voltage Measurement (section 4.8.3), there is described Gain Control Block (GCB). It mentions Vref in the Table 99., but this is related to PGA and not the ADC.

It looks like ADC reference voltage is fixed.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,624件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

looking at the datasheet it seems like it is not possible to change Vref.

In the Current and Voltage Measurement (section 4.8.3), there is described Gain Control Block (GCB). It mentions Vref in the Table 99., but this is related to PGA and not the ADC.

It looks like ADC reference voltage is fixed.

0 件の賞賛
返信