MFR4310 FlexRay

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFR4310 FlexRay

1,748件の閲覧回数
907439248
Contributor I

Hello, in the process of using MFR4310, channel A and B were configured in the tx slot, but in the actual work, channel A can communicate normally, but channel B has no data.The channel configuration and usage methods refer to the official routine.What might be the reason?Is it not supported by itself?

ラベル(1)
0 件の賞賛
返信
1 返信

1,680件の閲覧回数
nxa09859
NXP Employee
NXP Employee

Please check that the FlexRay controller is configured to work in the dual channel mode and that the channel B is enabled. Please, see the FR_MCR register for more details. Especially FR_MCR.SCM and FR_MCR.CHA and FR_MCR.CHB configuration.

0 件の賞賛
返信