MC9S12ZVML64MKH Code Warrior Processor Expert Generate Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12ZVML64MKH Code Warrior Processor Expert Generate Project

1,258件の閲覧回数
dannydeng
Contributor III

I used Code Warrior Processor Expert Generated a MC9S12ZVML64MKH  project to test the Phase voltage of BLDC, I configure all the function as attached file, but I got a static value while the phase voltage changed. Can anybody help me find the reason?

Thanks...

Original Attachment has been moved to: test.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,031件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Ray,

I shortly checked your code and unfortunately I do not see any obvious issue there.

The code should measure voltage at HS1 pin (pin49) divided by 6.

I didn’t test it till now.

Which voltage did you connect to HS1 pin?

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信