MC9S12ZV32 5V Output Current Max?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12ZV32 5V Output Current Max?

1,088件の閲覧回数
zongliangchan
Contributor I

VDDX pin maximum current?

if BCTL Control PNP Use BCP53-10(SOT223)

ラベル(1)
0 件の賞賛
返信
1 返信

937件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi Zong,

The current we can draw from the external ballast depends on the base current and gain of the  external ballast transistor.

The maximum current we can draw from external ballast transistor and supply VDDX rail is about power dissipation and thermal characteristics.

The user must ensure that the maximum junction temperature is not exceeded.

It depends on ambient temperature, thermal package characteristics and MCU power dissipation.

MCU power has to be calculated for the particular application. This is explained in RM section A.1.6.

For more details about this topic see application note below and section 3.2.2 PNP external ballast transistor:

  AN5084, Hardware Design Guidelines for S12ZVL Microcontrollers-Application n ... (REV 1) 

Regards,

iggi

0 件の賞賛
返信