MC9S12XEP100MAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12XEP100MAL

1,054 Views
L6550
Contributor I

I originally have a MC9S12G128 program that I want to port to the MC9S12XEP100MAL chip. After checking the information, I found that I need to use an expert system to build the program framework of the MC9S12XEP100MAL chip. I hope you can provide some information on building the program framework and the expert system APP. Thank you.

 

我本来有一款MC9S12G128程序要移植到MC9S12XEP100MAL这款芯片。查看资料发现要通过专家系统搭建MC9S12XEP100MAL这款芯片的程序框架,希望您能给予一些搭建程序框架的资料和专家系统的APP。谢谢您。

0 Kudos
Reply
1 Reply

1,034 Views
lama
NXP TechSupport
NXP TechSupport

Hi

The info you have is a little bit strange to me. You should start with HW and continue with SW step by step ...oscillator, and peripherals. Of course they are compatible but the S12XEP100 is a master device of successors S12XS, S12P, S12G (S12G is the simplest)

The most of routines will be just copy/paste but each must be checked.

https://community.nxp.com/t5/S12-MagniV-Microcontrollers/Reference-schematics-for-S12-X-devices/ta-p...

 

Attached differences ... S12G is more simplified S12P.

SW examples for S12XE

https://community.nxp.com/t5/S12-MagniV-Microcontrollers/LAMA-s-S12XE-unofficial-examples/ta-p/11007...

Compare memory map... attached

Best regards,

Ladislav

0 Kudos
Reply