MC9S12UF32 Speed Problems, please help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12UF32 Speed Problems, please help

2,275 Views
siebrand
Contributor I
Hello,

I need to have an Timer with 1Mhz. In this 1Mhz period I want do do something. That means the clock must be more than 1Mhz. I tested to toggle PORTB in an loop. Nothing else than this toggle. And on my osscilloscope I see 430Khz that means 1 operation will be operated at nearly 1Mhz. Didn't it have to be 12Mhz? The standart CLK of this MCU is 12Mhz or am I wrong?

And I should also be able to use the 60Mhz PLL Clock of the USB (PHY).

I tried many things like this:


CLKSEL = 0; // select OSC clock first, (PLLSEL = 0)

SYNR = 29; // Clock synthesizer divider (from VCO)
REFDV = 11; // Reference Clock source divider (from OSC)

asm{
nop
nop
nop
nop
};

PLLCTL_CME = 1;
PLLCTL_PLLON = 1;
PLLCTL_AUTO = 1;
PLLCTL_SCME = 1;

// Wait until PLL is locked
while (!CRGFLG_LOCK);

// Switch the SYSCLK to PLL Clk.
CLKSEL_PLLSEL = 1;


seen in the demo programm thumb drive or card reader. In these programms it is commented out, but in the doku it says it is right to to it like that.

It doesn't come out of the while and without it the speed is just slower. And the debugger stops at REFDV = 29 (or other than 0 values) but the programm runs. Just the debugger stops.

I hope someone has already experience with this board and speeds faster than the 12MHz it should have or the 1Mhz it have. Or some good explanation why one operation needs nearly 30 clocks.



Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,221 Views
siebrand
Contributor I
Ok I found the problem why I don't got the pll to work, because I don't activated the USB PLL.

UMCRH=0x40;

before the clk selection and pll settings

but I just get 2Mhz in an Loop with just toggling the portb. Shouldn't it be 60Mhz/4 (4 operations toggle portb and near jump and toggle portb back and jump again)
At 60Mhz one operation one clock should be 16,6ns. But it needs 250ns for setting a port and an near jmp.
this is my test programm for toggling the port (without the init. of the clock, before)

t:
PORTB ^= 0xff;
goto t;

I hope someone can help me with this problem, or explain me why.

Thanks
0 Kudos
Reply