MC9S12GN32MLC chip EEPROM module configuration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12GN32MLC chip EEPROM module configuration problem

Jump to solution
1,894 Views
jixiangli
Contributor III

Hello everyone! Thank you very much for answering my question!
I recently in the use of MC9S12GN32MLC chip, using this chip to do a car controller, due to the program upgrade, need to use the EEPROM module. I use the Processor Expert program, the following is my specific configuration, the EEPROM module shows the red exclamation mark, I put the wrong paste, please help me analyze the fault, thank you very much!!!

175564_175564.pngpastedImage_1.png

 

175589_175589.pngpastedImage_2.png

Labels (1)
0 Kudos
Reply
1 Solution
1,728 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Alt F7 -> Compiler for HCS12 -> Options -> Code Generation -> match PPAGE Register used for paging -> Write  RUNTIME into an empty cell below. -> OK -> Apply

pastedImage_1.png

Best regards,

Ladislav

View solution in original post

0 Kudos
Reply
2 Replies
1,729 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Alt F7 -> Compiler for HCS12 -> Options -> Code Generation -> match PPAGE Register used for paging -> Write  RUNTIME into an empty cell below. -> OK -> Apply

pastedImage_1.png

Best regards,

Ladislav

0 Kudos
Reply
1,728 Views
jixiangli
Contributor III

Thank you very much for your reply, help me to solve the problem, hope to make a friend, thank you!

0 Kudos
Reply