MC9S12G128 bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S12G128 bootloader

4,157 次查看
yongban
Contributor II

请教个问题:

在设计bootloader 之前,我在 9S12G128 app 代码:

按照AN4258 如下步骤改动:

  ROM_4000     = READ_ONLY     0x4000 TO   0x7F7F;  (文档是7F0F,对应的参考代码是7F7F

  ROM_C000     = READ_ONLY     0xC000 TO   0xEFDF;

/* paged FLASH:                     0x8000 TO   0xBFFF; addressed through PPAGE */
      PAGE_08       = READ_ONLY   0x088000 TO 0x08BFFF;
      PAGE_09       = READ_ONLY   0x098000 TO 0x09BFFF;
      PAGE_0A       = READ_ONLY   0x0A8000 TO 0x0ABFFF;
      PAGE_0B       = READ_ONLY   0x0B8000 TO 0x0BBFFF;
      PAGE_0C       = READ_ONLY   0x0C8000 TO 0x0C93FF;
      PAGE_0C_A000  = READ_ONLY   0x0CA000 TO 0x0CBFFF;
      PAGE_0E       = READ_ONLY   0x0E8000 TO 0x0EBFFF;
/*    PAGE_0D       = READ_ONLY   0x0D8000 TO 0x0DBFFF; not used: equivalent to ROM_4000 */
/*    PAGE_0F       = READ_ONLY   0x0F8000 TO 0x0FBEFF; not used: equivalent to ROM_C000 */
END

PLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */
      _PRESTART,              /* Used in HIWARE format: jump to _Startup at the code start */
      STARTUP,                /* startup data structures */
      ROM_VAR,                /* constant variables */
      STRINGS,                /* string literals */
      VIRTUAL_TABLE_SEGMENT,  /* C++ virtual table segment */
    //.ostext,                /* OSEK */
      NON_BANKED,             /* runtime routines which must not be banked */
      COPY                    /* copy down information: how to initialize variables */
                              /* in case you want to use ROM_4000 here as well, make sure
                                 that all files (incl. library files) are compiled with the
                                 option: -OnB=b */
                        INTO  ROM_C000/*, ROM_1400, ROM_4000*/;

      DEFAULT_ROM       INTO  PAGE_08, PAGE_09, PAGE_0A, PAGE_0B, PAGE_0C, PAGE_0C_A000, PAGE_0E 

 

void main(void)
{

 

  IVBR = 0x7F;
//set the vector base

 

改动后 程序无法正常运行,进去不了Main 函数;请问 还有哪里需要设置吗?

标签 (1)
0 项奖励
回复
4 回复数

2,921 次查看
920065012
Contributor II

hi,

    I meet the same question with you.How do you deal with it?

    I set the IVBR register( IVBR = 0x7F ),but the interrupt vector still at the 0xff80-0xffff. Where should I set the IVBR register,and what others should I do?

Regards,

Joy

0 项奖励
回复

2,921 次查看
iggi
NXP Employee
NXP Employee

Hi Yong,

Even we can use an online translator to translate your question, still it would be better if you can re-write it into English language.

Thanks,

iggi

0 项奖励
回复

2,921 次查看
yongban
Contributor II

Before design the bootloader ,I am changing 9S12G128 app code:

According AN4258 from NXP website

  ROM_4000     = READ_ONLY     0x4000 TO   0x7F7F;  (the document is 7F0F,but the code is 7F7F

  ROM_C000     = READ_ONLY     0xC000 TO   0xEFDF;

/* paged FLASH:                     0x8000 TO   0xBFFF; addressed through PPAGE */
      PAGE_08       = READ_ONLY   0x088000 TO 0x08BFFF;
      PAGE_09       = READ_ONLY   0x098000 TO 0x09BFFF;
      PAGE_0A       = READ_ONLY   0x0A8000 TO 0x0ABFFF;
      PAGE_0B       = READ_ONLY   0x0B8000 TO 0x0BBFFF;
      PAGE_0C       = READ_ONLY   0x0C8000 TO 0x0C93FF;
      PAGE_0C_A000  = READ_ONLY   0x0CA000 TO 0x0CBFFF;
      PAGE_0E       = READ_ONLY   0x0E8000 TO 0x0EBFFF;
/*    PAGE_0D       = READ_ONLY   0x0D8000 TO 0x0DBFFF; not used: equivalent to ROM_4000 */
/*    PAGE_0F       = READ_ONLY   0x0F8000 TO 0x0FBEFF; not used: equivalent to ROM_C000 */
END

PLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */
      _PRESTART,              /* Used in HIWARE format: jump to _Startup at the code start */
      STARTUP,                /* startup data structures */
      ROM_VAR,                /* constant variables */
      STRINGS,                /* string literals */
      VIRTUAL_TABLE_SEGMENT,  /* C++ virtual table segment */
    //.ostext,                /* OSEK */
      NON_BANKED,             /* runtime routines which must not be banked */
      COPY                    /* copy down information: how to initialize variables */
                              /* in case you want to use ROM_4000 here as well, make sure
                                 that all files (incl. library files) are compiled with the
                                 option: -OnB=b */
                        INTO  ROM_C000/*, ROM_1400, ROM_4000*/;

      DEFAULT_ROM       INTO  PAGE_08, PAGE_09, PAGE_0A, PAGE_0B, PAGE_0C, PAGE_0C_A000, PAGE_0E 

void main(void)
{

 

  IVBR = 0x7F;
//set the vector base

but after changing the code,the code can not work, Can not enter into the main ();  Is there where I need to set up?

0 项奖励
回复

2,921 次查看
iggi
NXP Employee
NXP Employee

Hi,

What did you change exactly?

The 0x7F7F is the max limit for ROM_4000 in the application project. Interrupt vector table is located at 0x7F80 - 0x7FFF.

So it doesn't matter if the limit is 0x7F7F or 0x7F0F, this should not have impact.

Have you done other modifications?

Regards,

iggi

0 项奖励
回复