MC68HC16Z1 behavior in LPSTOP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC68HC16Z1 behavior in LPSTOP

1,404件の閲覧回数
phil74
NXP Employee
NXP Employee

Hello,

 

My customer (Schneider) would like to get confirmation about MC68HC16Z1 spec and behavior in LPSTOP mode.

Can you help and confirm the following :

1/ During LPSTOP mode, the SIM is the only module that is still alive and is the only wakeup source with IRQ and PIT, or can some other modules (like GPT) wake up the MCU, depending of individual STOP bits in each module (ex : STOP bit in GPTMCR register) ?

 

2/ Assuming IC1 pin (GPT) is configured to generate an interrupt on edge.

While the MCU is  in LPSTOP mode, IC1 pin toggles once.

At wakeup, does the MCU will go to interrupt due to IC1 toggling during LPSTOP ?

 

Thanks in advance for your help,

Best Regards,

Philippe.

 

0 件の賞賛
返信
1 返信

1,314件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

As per the documentation,
1. Only PIT, IRQ and reset can bring the MCU from LPSTOP.

The stop bits can put individual modules into Stop mode without LPSTOP instruction.
2. GPT doesn’t wake up.

Regards,

Daniel

0 件の賞賛
返信