LIN one bit error signal

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN one bit error signal

ソリューションへジャンプ
2,206件の閲覧回数
itsnewforme
Contributor IV

Hi, In NXP Lin Stack there is a one bit error signal that is added to the Slave node I want to know what different type of error handling is done by the error Signal.

Thanks in advance.

タグ(3)
0 件の賞賛
返信
1 解決策
2,187件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi itsnewforme,

From my point of view, the response_error signal shall be set whenever a frame (except for event triggered frame responses) that is transmitted or received by the slave node contains an error(checksum error, framing error, readback error …) in the frame response. That means error signal will be set for all errors and we cannot distinguish which type of error based on error signal.

You can refer the chapter 2.7 of LIN_Specification_Package_2.2A.elf to detail.

Best regards,

Dan

元の投稿で解決策を見る

1 返信
2,188件の閲覧回数
DanNguyenDuy
NXP Employee
NXP Employee

Hi itsnewforme,

From my point of view, the response_error signal shall be set whenever a frame (except for event triggered frame responses) that is transmitted or received by the slave node contains an error(checksum error, framing error, readback error …) in the frame response. That means error signal will be set for all errors and we cannot distinguish which type of error based on error signal.

You can refer the chapter 2.7 of LIN_Specification_Package_2.2A.elf to detail.

Best regards,

Dan