LCD  MC9S12DP512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCD  MC9S12DP512

2,152 Views
dmomy
Contributor I
I'm trying to drive a 2X16 LCD from my MCU.  I'm using codewarrior 5.7  free version and processor expert.  I didn't see any beans for the LCD so I downloaded the ones on the PE site.  When I go to the processor expert bean description I could see the TLCD bean but when I go to   add the bean to my project it isn't visible. 
 
Is there a good example in C on how to drive the LCD if it isn't possible to use processor expert ?
 
Thanks

Dennis
 
 
 
Labels (1)
0 Kudos
Reply
1 Reply

1,154 Views
ProcessorExpert
Senior Contributor III
I'm sorry, but to use the additional beans available at Processor Expert website (e.g. TLCD) it's necessary to own at least the standard edition of the CodeWarrior. These beans are not supported in the special (free) edition.
0 Kudos
Reply