Issue with SCI interface with LIN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with SCI interface with LIN

1,199 次查看
vamsichakravart
Contributor I

I am using sci peripheral in mc9s12gN16 20 pin package for interfacing with LIN peripheral.I am not getting Rx interrupt atleast even Errors(like frame,overflow) also.Kindly provide the value of initialization registers  and let me know if there are any issues u faced with SCI interfacing with LIN.

标签 (1)
0 项奖励
回复
1 回复

1,090 次查看
RadekS
NXP Employee
NXP Employee

Hi vamsi,

The basic requirement is that LIN transceiver must be enabled. Therefore you need provide 12V power supply to LIN transceiver.

If you use TWR-S12GN32 board:

1.    please connect 12V to E1, E2 connector

2.    route RXD0 and TXD0 signals to LIN transceiver – jumpers 1-3 and 2-4 at JP1

3.    if your node will be LIN master, please connect jumper 3-4 at JP3

4.    if you want provide 12V power to next node over LIN cable, please connect jumper 1-2 at JP3.

The simple LIN example code could be downloaded from here:

https://community.freescale.com/docs/DOC-93792


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复