Is it necessary to use PDO and PDOCLK for debugging and downloading the S912ZVML32F3MKH chip program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it necessary to use PDO and PDOCLK for debugging and downloading the S912ZVML32F3MKH chip program

1,685 Views
yankui666
Contributor III

I am using the S912ZVML32F3MKH chip. If I don't use the PDO and PDOCLK pins and only use BKCD, RST, GND, and VDDX, can I debug and download the program properly. Do PDO
and PDOCLK require a download port to debug the download program?

0 Kudos
Reply
3 Replies

523 Views
fnfunkin
Contributor I

I used Multilink with CodeWarrior to flash firmware, and once I had the right drivers and properly set up the BKCD, RST, GND, and VDDX connections, it worked smoothly. The trickiest part was configuring the target setup—felt like an FNF rhythm check: mess up one beat (or pin), and nothing syncs. P&E Micro’s docs and example projects helped a lot, but expect a bit of trial and error at first.

0 Kudos
Reply

1,655 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

 

We recommend using all the necessary pins so that all debugging functions are available. You don't know if you'll ever need it and then you'll miss it. For example, the trace function. In addition, the debugger can have a property implemented when it needs these pins. We don't see it because it is given by the implementation of the debug interface, its protocol and properties, which is not our product. Of course, if you check your specific usage, then the possibility is there, but as I already wrote, it is better to use the full interface.

Best regards,

Ladislav

0 Kudos
Reply

810 Views
emilio
Contributor I
If I have the Multilink ans Codewarrior, how can I download the firmware?, any sample project or documentation related, how can I do?
I am try to use BKCD, RST, GND, and VDDX.
0 Kudos
Reply