Interface MAX3420E to MC9s12c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface MAX3420E to MC9s12c

1,990 Views
tnriley
Contributor III
Does anyone have experience with using the MAX3420E part? In particular, I need some example code for interfacing with the MC9s12c part. Thanks.
Labels (1)
0 Kudos
Reply
2 Replies

1,466 Views
KH_SRNL
Contributor I

Not yet, but I'm working on the same problem.  Maxim usually does a pretty good job of documenting their parts, but this one doesn't appear to have all of the information in one concise location.  If you look at App Note 3637 on the Maxim website (Add USB to Anything), there is a code sample attached to this app note that details most of what you need (I think).  The code with the app note does a decent job of explaining the various code parts.

 

If you do find a better sample code, please post it.  I'd like to see it as well.

0 Kudos
Reply

1,466 Views
tnriley
Contributor III

Yea, I have been looking through that one as well. There are just a few anoying things like missing header files and such that make it a little frustrating to deal with. The do have a programming Guide that explains the register defines as well a few other documents, but no complete top to bottom examples.

 

http://www.maxim-ic.com/app-notes/index.mvp/id/3598

http://application-notes.digchip.com/003/3-5613.pdf

 

Also, I have not yet tried out the windows interface end. I have tried the eval board app with wordpad just to verify that the device would work, but nothing else to date.

0 Kudos
Reply