Inquiry of CW development studi0 11.1 connection issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry of CW development studi0 11.1 connection issue

651 Views
eric2lim
Contributor I

Hello,

I've set up Codewarrior Development Studio 11.1 and then connected MultiLink Universal FX to my S12ZVL MCU board.

First of all, my project is passed clean and build process well.

By the way, when I tried to change to debug mode, error popup window displayed..

I attached related log files.

I hope this environment issue will be solved soon.

Best regards.

eric Lim (limbcho_2@hotmail.com)

0 Kudos
Reply
1 Reply

591 Views
stanish
NXP Employee
NXP Employee

Hello,

thanks for your report.

Could you possibly try to create a new project using " New Project Wizard"?

Please try to build and debug the "Empty" project -> This will help to distingusih if there is a project related corruption or rather the installer is missing some component or is corrupted.

If the new project does not work neither I'd suggest you to re-download and re-install CW for MCU v 11.1 as a administrator on your machine.

Hope it helps.

Stan

 

 

0 Kudos
Reply