In MC9S12X, stop sending the error frames in CAN Bus-Off state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In MC9S12X, stop sending the error frames in CAN Bus-Off state

3,198件の閲覧回数
Nash_win
Contributor I

Currently I am using the Auto Bus-Off recovery feature of MSCAN of MC9S12X.

However, the problem with this is that when the Bus-Off occurs, due to the auto-recovery, the uC starts sending the error frames continuously in the Bus-Off state.

If i want to stop the Error frames for certain period, how can i do it?

ラベル(1)
2 返答(返信)

2,824件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

It looks like you are going into the same error after buss off recovery. If the MCU is in the bus off then it does not sends any frames. A bus-off node is not allowed to have any influence on the bus (e.g. output drivers switched off). It looks like you are facing behavior presented in attached files.

What I would like to suggest you is to abort the messages and fix all mistakes:

if (CAN0TFLG != 0x07)

{

  do

    {

      if( !CAN0TFLG_TXE0 )

         {   CAN0TARQ_ABTRQ0 =  1; // abort the transmission

              while ( ! CAN0TAAK_ABTAK0 ) {}

        }

       if( !CAN0TFLG_TXE1 )

          {   CAN0TARQ_ABTRQ1 =  1; // abort the transmission

               while ( ! CAN0TAAK_ABTAK1 ) {}

           }

       if( !CAN0TFLG_TXE2 )

          {   CAN0TARQ_ABTRQ2 =  1; // abort the transmission

               while ( ! CAN0TAAK_ABTAK2 ) {}

          }

    }

while(CAN0TFLG != 7);

}

Best Regards, Ladislav

0 件の賞賛
返信

2,824件の閲覧回数
howardg
Contributor II

Ladislav, do you know whether this technique should fail on the KE06?  I tried it,  modified for the different register names, but I'm not consistently getting bus-off interrupts with the KE06's MSCAN peripheral.  After a bus off interrupt and abort I back off for 5 seconds and then try again.  I can do that twice before the KE06/MSCAN gives up and stops generating bus off interrupts.

0 件の賞賛
返信