I need a sample schematic using the MC9S12DT128. My circuit I designed isn't working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need a sample schematic using the MC9S12DT128. My circuit I designed isn't working.

969 Views
gerryhermann
Contributor I

I designed a circuit around the MC9S12DT128BMPV. I'm using an external 16MHz clock. When I power up there are some erratic square wave signals on the I/O pins. It seems like it is going through some type of continuous reset. I have the reset line pulled high with a 5K resistor. CW with a Cyclone can't communicate. Any ideas?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

820 Views
iggi
NXP Employee
NXP Employee

Hi Gerry,

I would like to recommend you an app note, the AN2727 Designing Hardware for the HCS12 D-Family:

cache.freescale.com/files/microcontrollers/doc/app_note/AN2727.pdf

Kindly go through it and check if you have anything different than stated in the app note such as:

- Power supply connections

- Control pin connections

- Oscillator options

etc.

Regards,
iggi

0 Kudos
Reply