How to write MC9S12DG128B MCU Interrupt Service Program without Interrupt Number

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to write MC9S12DG128B MCU Interrupt Service Program without Interrupt Number

2,137 次查看
commandoccz
Contributor I
How to write MC9S12DG128B MCU Interrupt Service Program without Interrupt Number
But use the Interrupt Vector Table that defined in the mc9s12gd128.h file
Thanks~~~~
标签 (1)
0 项奖励
回复
1 回复

1,287 次查看
JimDon
Senior Contributor III
Here us a link to a file with the code.


Code: // This is code generated by Processor Expert automatically. // Un-used interrupt ISR(Cpu_Interrupt) {   asm(BGND); }
/* ISR prototype */typedef void (*near tIsrFunc)(void);const tIsrFunc _InterruptVectorTable[] @0xFF80 = { /* Interrupt vector table */  /* ISR name                               No. Address Pri Name          Description */  Cpu_Interrupt,                       /* 0x3F  0xFF80   1  ivVReserved63 unused by PE */  Cpu_Interrupt,                       /* 0x3E  0xFF82   1  ivVReserved62 unused by PE */  Cpu_Interrupt,                       /* 0x3D  0xFF84   1  ivVReserved61 unused by PE */  Cpu_Interrupt,                       /* 0x3C  0xFF86   1  ivVReserved60 unused by PE */  Cpu_Interrupt,                       /* 0x3B  0xFF88   1  ivVReserved59 unused by PE */  Cpu_Interrupt,                       /* 0x3A  0xFF8A   1  ivVReserved58 unused by PE */  Cpu_Interrupt,                       /* 0x39  0xFF8C   1  ivVpwmesdn    unused by PE */  Cpu_Interrupt,                       /* 0x38  0xFF8E   1  ivVportp      unused by PE */  Cpu_Interrupt,                       /* 0x37  0xFF90   1  ivVcan4tx     unused by PE */  Cpu_Interrupt,                       /* 0x36  0xFF92   1  ivVcan4rx     unused by PE */  Cpu_Interrupt,                       /* 0x35  0xFF94   1  ivVcan4err    unused by PE */  Cpu_Interrupt,                       /* 0x34  0xFF96   1  ivVcan4wkup   unused by PE */  Cpu_Interrupt,                       /* 0x33  0xFF98   1  ivVReserved51 unused by PE */  Cpu_Interrupt,                       /* 0x32  0xFF9A   1  ivVReserved50 unused by PE */  Cpu_Interrupt,                       /* 0x31  0xFF9C   1  ivVReserved49 unused by PE */  Cpu_Interrupt,                       /* 0x30  0xFF9E   1  ivVReserved48 unused by PE */  Cpu_Interrupt,                       /* 0x2F  0xFFA0   1  ivVReserved47 unused by PE */  Cpu_Interrupt,                       /* 0x2E  0xFFA2   1  ivVReserved46 unused by PE */  Cpu_Interrupt,                       /* 0x2D  0xFFA4   1  ivVReserved45 unused by PE */  Cpu_Interrupt,                       /* 0x2C  0xFFA6   1  ivVReserved44 unused by PE */  Cpu_Interrupt,                       /* 0x2B  0xFFA8   1  ivVReserved43 unused by PE */  Cpu_Interrupt,                       /* 0x2A  0xFFAA   1  ivVReserved42 unused by PE */  Cpu_Interrupt,                       /* 0x29  0xFFAC   1  ivVReserved41 unused by PE */  Cpu_Interrupt,                       /* 0x28  0xFFAE   1  ivVReserved40 unused by PE */  Cpu_Interrupt,                       /* 0x27  0xFFB0   1  ivVcan0tx     unused by PE */  Cpu_Interrupt,                       /* 0x26  0xFFB2   1  ivVcan0rx     unused by PE */  Cpu_Interrupt,                       /* 0x25  0xFFB4   1  ivVcan0err    unused by PE */  Cpu_Interrupt,                       /* 0x24  0xFFB6   1  ivVcan0wkup   unused by PE */  Cpu_Interrupt,                       /* 0x23  0xFFB8   1  ivVflash      unused by PE */  Cpu_Interrupt,                       /* 0x22  0xFFBA   1  ivVeeprom     unused by PE */  Cpu_Interrupt,                       /* 0x21  0xFFBC   1  ivVReserved33 unused by PE */  Cpu_Interrupt,                       /* 0x20  0xFFBE   1  ivVspi1       unused by PE */  Cpu_Interrupt,                       /* 0x1F  0xFFC0   1  ivViic        unused by PE */  Cpu_Interrupt,                       /* 0x1E  0xFFC2   1  ivVReserved30 unused by PE */  Cpu_Interrupt,                       /* 0x1D  0xFFC4   1  ivVcrgscm     unused by PE */  Cpu_Interrupt,                       /* 0x1C  0xFFC6   1  ivVcrgplllck  unused by PE */  Cpu_Interrupt,                       /* 0x1B  0xFFC8   1  ivVtimpabovf  unused by PE */  Cpu_Interrupt,                       /* 0x1A  0xFFCA   1  ivVtimmdcu    unused by PE */  Cpu_Interrupt,                       /* 0x19  0xFFCC   1  ivVporth      unused by PE */  Cpu_Interrupt,                       /* 0x18  0xFFCE   1  ivVportj      unused by PE */  Cpu_Interrupt,                       /* 0x17  0xFFD0   1  ivVatd1       unused by PE */  Cpu_Interrupt,                       /* 0x16  0xFFD2   1  ivVatd0       unused by PE */  Cpu_Interrupt,                       /* 0x15  0xFFD4   1  ivVsci1       unused by PE */  Cpu_Interrupt,                       /* 0x14  0xFFD6   1  ivVsci0       unused by PE */  Cpu_Interrupt,                       /* 0x13  0xFFD8   1  ivVspi0       unused by PE */  Cpu_Interrupt,                       /* 0x12  0xFFDA   1  ivVtimpaie    unused by PE */  Cpu_Interrupt,                       /* 0x11  0xFFDC   1  ivVtimpaaovf  unused by PE */  Cpu_Interrupt,                       /* 0x10  0xFFDE   1  ivVtimovf     unused by PE */  Cpu_Interrupt,                       /* 0x0F  0xFFE0   1  ivVtimch7     unused by PE */  Cpu_Interrupt,                       /* 0x0E  0xFFE2   1  ivVtimch6     unused by PE */  Cpu_Interrupt,                       /* 0x0D  0xFFE4   1  ivVtimch5     unused by PE */  Cpu_Interrupt,                       /* 0x0C  0xFFE6   1  ivVtimch4     unused by PE */  Cpu_Interrupt,                       /* 0x0B  0xFFE8   1  ivVtimch3     unused by PE */  Cpu_Interrupt,                       /* 0x0A  0xFFEA   1  ivVtimch2     unused by PE */  Cpu_Interrupt,                       /* 0x09  0xFFEC   1  ivVtimch1     unused by PE */  Cpu_Interrupt,                       /* 0x08  0xFFEE   1  ivVtimch0     unused by PE */  Cpu_Interrupt,                       /* 0x07  0xFFF0   1  ivVrti        unused by PE */  Cpu_Interrupt,                       /* 0x06  0xFFF2   1  ivVirq        unused by PE */  Cpu_Interrupt,                       /* 0x05  0xFFF4   -  ivVxirq       unused by PE */  Cpu_Interrupt,                       /* 0x04  0xFFF6   -  ivVswi        unused by PE */  Cpu_Interrupt,                       /* 0x03  0xFFF8   -  ivVtrap       unused by PE */  /* Reset handler name */  _EntryPoint,                         /* 0x02  0xFFFA   -  ivVcop        unused by PE */  _EntryPoint,                         /* 0x01  0xFFFC   -  ivVclkmon     unused by PE */  _EntryPoint                          /* 0x00  0xFFFE   -  ivVreset      used by PE */};
 


Message Edited by JimDon on 2008-04-01 10:30 AM
0 项奖励
回复