How to use active crystal?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use active crystal?

1,359 Views
407214944
Contributor I

      In our project, MC9S128G is used as a single chip microcomputer. The clock USES 3.3V active crystal vibration, and the crystal oscillator output end adopts two resistance partial pressures, reducing the output clock amplitude to below 1.8V, about 1V.But the debugging finds that it is stuck at the while(CPMUFLG_LOCK==0);That is, PLL never locks.Can you provide a bit of this single chip to use active crystal to use.Thank you very much!

0 Kudos
Reply
1 Reply

1,211 Views
lama
NXP TechSupport
NXP TechSupport

Before you use PLL be sure the oscillator is working correctly.

1. Use normal passive crystal. (oscillator) Active, are not supported by S12G device.

2. To check correct behavior, use PBE mode and you should measure frequency of BUSCLK=OSCCLK/2 at ECLK pin. Of course you have to set ECLKCTL_NECLK=0. This says you, without measurement, whether your oscillator works.

The data sheet states:

pastedImage_1.png

C: Those parameters are achieved by the design characterization by measuring a statistically relevant sample size across process variations.
D: Those parameters are derived mainly from simulations

The PLL setup for different modes: https://community.nxp.com/docs/DOC-93792 

Best regards,

Ladislav

0 Kudos
Reply