How to use CW create .hex file to program freescale SZ12 micro without source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use CW create .hex file to program freescale SZ12 micro without source code

2,556件の閲覧回数
jvm_jh
Contributor I

Is there anyway to generate .hex file from CW? Try to pass the simple file for flashing controllers.

Or CW provide any other format files to support direct flashing process? Just don't want technician deal with source code and compiling/ debugging process. 

Thank you for the help!

タグ(4)
3 返答(返信)

2,405件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello John Huang,

In CodeWarrior 10.x or 11, can generate S-Record file :

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,405件の閲覧回数
jvm_jh
Contributor I

Thank you, Alice, for the tips. 

0 件の賞賛
返信

2,405件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi John,

Welcome.

BR

Alice

0 件の賞賛
返信