How to use CW create .hex file to program freescale SZ12 micro without source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use CW create .hex file to program freescale SZ12 micro without source code

2,557 Views
jvm_jh
Contributor I

Is there anyway to generate .hex file from CW? Try to pass the simple file for flashing controllers.

Or CW provide any other format files to support direct flashing process? Just don't want technician deal with source code and compiling/ debugging process. 

Thank you for the help!

3 Replies

2,406 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello John Huang,

In CodeWarrior 10.x or 11, can generate S-Record file :

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,406 Views
jvm_jh
Contributor I

Thank you, Alice, for the tips. 

0 Kudos
Reply

2,406 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi John,

Welcome.

BR

Alice

0 Kudos
Reply