How to use CAN 2.0A/2.0B for S12ZVC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use CAN 2.0A/2.0B for S12ZVC?

跳至解决方案
1,480 次查看
aaronlee
Contributor V

Hi,

I use CAN 2.0A on S12ZVCA. It work fine @ 250kbps CAN and 12MHz crystal. (My code as attachments, The example code follow MSCAN on the MagniV (AN4975) with software.)

Now, I want to use CAN 2.0A and 2.0B together.

Do you have example code?

Best Regards,

Aaron

标记 (1)
0 项奖励
回复
1 解答
1,125 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

CAN 2.A and 2.0B compatibility:

Source: https://www.opal-rt.com/KMP/index.php?/article/AA-00691/0/Opal-RT-CAN-solution-compatibility-with-CA...

CAN specifies two different formats for the Arbitration ID parameter. The standard message format uses a 11-bit ID, while the extended message format uses a 29-bit ID.

CAN 2.0A                 - specifies standard message format only (extended messages are treated as an error)
CAN 2.0B passive    - handles standard messages and ignores extended messages
CAN 2.0B active      - handles both standard and extended message formats

Opal-RT's hardware and software is 2.0B active compliant: it supports both standard (11-bit) and extended (29-bit) Arbitration IDs.

The following table displays the different versions of the CAN standard, the year they were adopted, and a brief synopsis of the changes made with each revision.

Version    Year       Additions
1.0           1995       Original CAN standard
1.1           1987       Respecified bit timing requirements
1.2           1990       Increased oscillator tolerance
2.0A         1991       Same as version 1.2
2.0B         1991       Introduced optional extended frame

 

The example for https://www.nxp.com/docs/en/application-note/AN4975.pdf

Together with https://www.nxp.com/docs/en/application-note-software/AN4975SW.zip

Simple example for CAN standard ID and loopback mode is attached.

best regards,

Ladislav

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,126 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

CAN 2.A and 2.0B compatibility:

Source: https://www.opal-rt.com/KMP/index.php?/article/AA-00691/0/Opal-RT-CAN-solution-compatibility-with-CA...

CAN specifies two different formats for the Arbitration ID parameter. The standard message format uses a 11-bit ID, while the extended message format uses a 29-bit ID.

CAN 2.0A                 - specifies standard message format only (extended messages are treated as an error)
CAN 2.0B passive    - handles standard messages and ignores extended messages
CAN 2.0B active      - handles both standard and extended message formats

Opal-RT's hardware and software is 2.0B active compliant: it supports both standard (11-bit) and extended (29-bit) Arbitration IDs.

The following table displays the different versions of the CAN standard, the year they were adopted, and a brief synopsis of the changes made with each revision.

Version    Year       Additions
1.0           1995       Original CAN standard
1.1           1987       Respecified bit timing requirements
1.2           1990       Increased oscillator tolerance
2.0A         1991       Same as version 1.2
2.0B         1991       Introduced optional extended frame

 

The example for https://www.nxp.com/docs/en/application-note/AN4975.pdf

Together with https://www.nxp.com/docs/en/application-note-software/AN4975SW.zip

Simple example for CAN standard ID and loopback mode is attached.

best regards,

Ladislav

0 项奖励
回复