Hi,
I use CAN 2.0A on S12ZVCA. It work fine @ 250kbps CAN and 12MHz crystal. (My code as attachments, The example code follow MSCAN on the MagniV (AN4975) with software.)
Now, I want to use CAN 2.0A and 2.0B together.
Do you have example code?
Best Regards,
Aaron
已解决! 转到解答。
Hi,
CAN 2.A and 2.0B compatibility:
CAN specifies two different formats for the Arbitration ID parameter. The standard message format uses a 11-bit ID, while the extended message format uses a 29-bit ID.
CAN 2.0A - specifies standard message format only (extended messages are treated as an error)
CAN 2.0B passive - handles standard messages and ignores extended messages
CAN 2.0B active - handles both standard and extended message formats
Opal-RT's hardware and software is 2.0B active compliant: it supports both standard (11-bit) and extended (29-bit) Arbitration IDs.
The following table displays the different versions of the CAN standard, the year they were adopted, and a brief synopsis of the changes made with each revision.
Version Year Additions
1.0 1995 Original CAN standard
1.1 1987 Respecified bit timing requirements
1.2 1990 Increased oscillator tolerance
2.0A 1991 Same as version 1.2
2.0B 1991 Introduced optional extended frame
The example for https://www.nxp.com/docs/en/application-note/AN4975.pdf
Together with https://www.nxp.com/docs/en/application-note-software/AN4975SW.zip
Simple example for CAN standard ID and loopback mode is attached.
best regards,
Ladislav
Hi,
CAN 2.A and 2.0B compatibility:
CAN specifies two different formats for the Arbitration ID parameter. The standard message format uses a 11-bit ID, while the extended message format uses a 29-bit ID.
CAN 2.0A - specifies standard message format only (extended messages are treated as an error)
CAN 2.0B passive - handles standard messages and ignores extended messages
CAN 2.0B active - handles both standard and extended message formats
Opal-RT's hardware and software is 2.0B active compliant: it supports both standard (11-bit) and extended (29-bit) Arbitration IDs.
The following table displays the different versions of the CAN standard, the year they were adopted, and a brief synopsis of the changes made with each revision.
Version Year Additions
1.0 1995 Original CAN standard
1.1 1987 Respecified bit timing requirements
1.2 1990 Increased oscillator tolerance
2.0A 1991 Same as version 1.2
2.0B 1991 Introduced optional extended frame
The example for https://www.nxp.com/docs/en/application-note/AN4975.pdf
Together with https://www.nxp.com/docs/en/application-note-software/AN4975SW.zip
Simple example for CAN standard ID and loopback mode is attached.
best regards,
Ladislav