How to trap execution of unused memory in EEPROM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to trap execution of unused memory in EEPROM?

1,118件の閲覧回数
ramakrishnaredd
Contributor I


execution of unused memory

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,043件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

As I mentioned before, you should share type of the MCU. The reason is that, for example in the case of S12X MCUs you can use MPU module to check accesses.

BR

Ladislav

0 件の賞賛
返信

1,043件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

You have not mentioned type of the MCU, however I have one idea.

You should use FILL command  in the for all unused memory in the prm file.

Example from a CodeWarrior IDE help

SEGMENTS

     RAM_1  = READ_WRITE 0x800 TO 0x8FF

              FILL 0xAA 0x55;

END

PLACEMENT

     DUMMY  INTO RAM_1

END

I suggest you to use filling value 0x3F which is code for assembler SWI instruction.

Then you should create interrupt routine to be able to service SWI.

When SWI then happens you can check stack and read from it an address from which you have jumped to SWI interrupt.

If you want to read stack you will have to use ASM instructions.

 

Best Regards, Ladislav

0 件の賞賛
返信