I am programming the function of writing and reading data from D-Flash of the mc9s12xs128maa.
It seem that i can erase and write the sector because the FSTAT is 0x80 after i called Flash_Erase() and Flash_Write(),but i don't konw how to read the data from D-Flash.Could someone help me?
Here is my code:
void Flash_Init()
{
FCLKDIV=0x0f;
DFPROT=0x80;
}
void Flash_Erase() {
DisableInterrupts;
if ((FSTAT & 0x30) != 0) {
FSTAT |= 0x30; // clear ACCERR or FPVIOL if set
}
FCCOBIX = 0x00; /* index 0 */
FCCOBHI = 0x12; /* D-Flash Erase command */
FCCOBLO = 0x10; /* Global address value i.e. G-Page value */
FCCOBIX = 0x01; /* index 1 */
FCCOB = 0x0f00; /* sector address of a D-Flash */
FSTAT = 0x80;
while(!FSTAT_CCIF);
EnableInterrupts;
}
void Flash_Write(unsigned char address){
DisableInterrupts;
while(FSTAT_CCIF==0) ;
if ((FSTAT & 0x30) != 0) {
FSTAT |= 0x30; // clear ACCERR or FPVIOL if set
}
FCCOBIX = 0;
FCCOBHI = 0x11; // prog D-flash
FCCOBLO = 0x10; // global addr
FCCOBIX = 1;
FCCOB = 0x0f00; //global addr - within an erased sectot
FCCOBIX = 2;
FCCOB = 0xabab;
FCCOBIX = 3;
FCCOB = 0xabab;
FSTAT = 0x80;
while(!FSTAT_CCIF);
EnableInterrupts;
}
word Flash_Read(unsigned char address){
word *p;
p=(word*)(0x100f00);
return *p;
}
Flash_Init();
Flash_Erase();
Flash_Write(0);
Flash_Read(0);
called in main.
thinks.
已解决! 转到解答。
I had solved the problem by myself. Originally, we should set the EPAGE register to determine which D-Flash sector map the local address in 0x0800 that is used as a D-Flash window to access globle address from 0x10000 to 0x101fff.
Here is my code.
void Flash_Init()
{
FCLKDIV=0x0f;
DFPROT=0x80;
EPAGE=0x00;
}
void Flash_Erase() {
DisableInterrupts;
if ((FSTAT & 0x30) != 0) {
FSTAT |= 0x30; // clear ACCERR or FPVIOL if set
}
FCCOBIX = 0x00; /* index 0 */
FCCOBHI = 0x12; /* D-Flash Erase command */
FCCOBLO = 0x10; /* Global address value i.e. G-Page value */
FCCOBIX = 0x01; /* index 1 */
FCCOB = 0x0000; /* sector address of a D-Flash */
FSTAT = 0x80;
while(!FSTAT_CCIF);
EnableInterrupts;
}
void Flash_Write(unsigned char address,word value){
DisableInterrupts;
while(FSTAT_CCIF==0) ;
if ((FSTAT & 0x30) != 0) {
FSTAT |= 0x30; // clear ACCERR or FPVIOL if set
}
FCCOBIX = 0;
FCCOBHI = 0x11; // prog D-flash
FCCOBLO = 0x10; // global addr
FCCOBIX = 1;
FCCOB = 0x0000+address; //global addr - within an erased sectot
FCCOBIX = 2;
FCCOB = value;
FSTAT = 0x80;
while(!FSTAT_CCIF);
EnableInterrupts;
}
unsigned char Flash_Read(unsigned char address){
unsigned char *p;
p=(unsigned char*)(0x0800+address);
return *p;
}
Because i only have 10 foat-data to store, i just implement a sector of D-Flash which has 256byte.
I had solved the problem by myself. Originally, we should set the EPAGE register to determine which D-Flash sector map the local address in 0x0800 that is used as a D-Flash window to access globle address from 0x10000 to 0x101fff.
Here is my code.
void Flash_Init()
{
FCLKDIV=0x0f;
DFPROT=0x80;
EPAGE=0x00;
}
void Flash_Erase() {
DisableInterrupts;
if ((FSTAT & 0x30) != 0) {
FSTAT |= 0x30; // clear ACCERR or FPVIOL if set
}
FCCOBIX = 0x00; /* index 0 */
FCCOBHI = 0x12; /* D-Flash Erase command */
FCCOBLO = 0x10; /* Global address value i.e. G-Page value */
FCCOBIX = 0x01; /* index 1 */
FCCOB = 0x0000; /* sector address of a D-Flash */
FSTAT = 0x80;
while(!FSTAT_CCIF);
EnableInterrupts;
}
void Flash_Write(unsigned char address,word value){
DisableInterrupts;
while(FSTAT_CCIF==0) ;
if ((FSTAT & 0x30) != 0) {
FSTAT |= 0x30; // clear ACCERR or FPVIOL if set
}
FCCOBIX = 0;
FCCOBHI = 0x11; // prog D-flash
FCCOBLO = 0x10; // global addr
FCCOBIX = 1;
FCCOB = 0x0000+address; //global addr - within an erased sectot
FCCOBIX = 2;
FCCOB = value;
FSTAT = 0x80;
while(!FSTAT_CCIF);
EnableInterrupts;
}
unsigned char Flash_Read(unsigned char address){
unsigned char *p;
p=(unsigned char*)(0x0800+address);
return *p;
}
Because i only have 10 foat-data to store, i just implement a sector of D-Flash which has 256byte.