How to measure clock cycles/ timing in true time simulator/ Real-time debugger between breakpoints

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to measure clock cycles/ timing in true time simulator/ Real-time debugger between breakpoints

跳至解决方案
2,205 次查看
ramakr02
Contributor III

Dear All,

Following are the details of the hardware used:

1. Development board: EVB9S12XF512E (S12XFSTARTERKITE: S12XF 2-Node Starter Kit)

2. Target Processor: MC9S12XF512MLM

3. IDE: CodeWarrior Classic HCS12(X) 5.2 (Added the missing derivatives)

I was wondering if there is any debugger option or tool within true time simulator/ Real-time debugger to count or measure clock cycles (or time) elapsed between a breakpoint or start and stop of program on-board?

Any help is welcome!   @dianabatrlova , @RadekS 

Thank you.

Best regards,

Rohit

0 项奖励
回复
1 解答
2,192 次查看
RadekS
NXP Employee
NXP Employee

Hi ramakr02,

You may switch hiwave into Full Chip Simulation (menu-Component-Set Connection). 
The Register window will show clock cycles. You may switch to the time axis (in ms) by click on the clock value at the Status bar. This tool is good mainly for testing limited code snippets due to a lack of interrupts.

Unfortunately, no clock counter directly in CPU which may be used in run-time debugging on MCU. You may configure and use TCNT register for measuring time periods. However, we typically use an Oscilloscope or Logic Analyzer together with GPIO pin toggling for time measurement.

The GPIO pin toggling presents minimum code intervention and known self-compensated delay for port write.  

I hope it helps you.

Best regards

Radek

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,193 次查看
RadekS
NXP Employee
NXP Employee

Hi ramakr02,

You may switch hiwave into Full Chip Simulation (menu-Component-Set Connection). 
The Register window will show clock cycles. You may switch to the time axis (in ms) by click on the clock value at the Status bar. This tool is good mainly for testing limited code snippets due to a lack of interrupts.

Unfortunately, no clock counter directly in CPU which may be used in run-time debugging on MCU. You may configure and use TCNT register for measuring time periods. However, we typically use an Oscilloscope or Logic Analyzer together with GPIO pin toggling for time measurement.

The GPIO pin toggling presents minimum code intervention and known self-compensated delay for port write.  

I hope it helps you.

Best regards

Radek

 

0 项奖励
回复
2,190 次查看
ramakr02
Contributor III

Thank you @RadekS .

 

I've configured PIT1 for 20usec period, just wanted to confirm that period in debugger. Oscilloscope is an option. 

 

Also, I think the flexray module on chip, is not halted when true time simulator is paused. Is that true?  

 

Best regards,

Rohit

0 项奖励
回复