How to library Download?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to library Download?

ソリューションへジャンプ
2,859件の閲覧回数
Kr_Blue
Contributor I

hI all.

 

I had the flash and related programs.

 

However, this definition is in the library FADDR FDATA and it is not.

I think this library is not update.

 

I want to Download to library. So Search to library and not find.

 

How to Download that?


Chip : MC9S12DJ128 VPV

 

  

ラベル(1)
0 件の賞賛
返信
1 解決策
2,380件の閲覧回数
CrasyCat
Specialist III

Hello

 

According to my understanding you are using CodeWarrior for HC12 V5.1 and you are missing definition of registers  FADDR and FDATA in mc9s12dj128.c / mc9s12dj128.h/

 

I checked the delivered files and the definition for these registers are indeed missing.

 

I would recommend you to submit a service request to get that fixed.
Click here to submit a service request.

In the mean time you can add register definition from attached regdef.h and refdef.c respectively to your mc9s12dj128.h and mc9s12dj128.c files.

 

These files are located respectively in directory {Install}\lib\hc12c\include and {Install}\lib\hc12c\src.

 


CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,381件の閲覧回数
CrasyCat
Specialist III

Hello

 

According to my understanding you are using CodeWarrior for HC12 V5.1 and you are missing definition of registers  FADDR and FDATA in mc9s12dj128.c / mc9s12dj128.h/

 

I checked the delivered files and the definition for these registers are indeed missing.

 

I would recommend you to submit a service request to get that fixed.
Click here to submit a service request.

In the mean time you can add register definition from attached regdef.h and refdef.c respectively to your mc9s12dj128.h and mc9s12dj128.c files.

 

These files are located respectively in directory {Install}\lib\hc12c\include and {Install}\lib\hc12c\src.

 


CrasyCat

0 件の賞賛
返信
2,380件の閲覧回数
Kr_Blue
Contributor I

Thank you for your advice.

 

Attached file is very useful !!

0 件の賞賛
返信
2,380件の閲覧回数
kef
Specialist I

I think it is quite OK that FADDR and FDATA are not listed in derivative files. FADDR and FDATA can be used only in special modes and thus are not useful for real life applications. Only BDM debuggers/programmers can use FDATA and FADDR for erase/program operations. Users applications have to write directly into flash array.

0 件の賞賛
返信