How to encrypt the 9S12 singlechip?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to encrypt the 9S12 singlechip?

2,718 Views
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Mon Jun 27, 2005 5:55 am    
 
Dear Sir:
Thanks for your help. And now we are useing the 9S12 controller,but how to encrypt my program when I download them into the chips? I know that HC908 serias singlechip has the function of encrypt when burning the program into chips. And if the 9S12 singlechip also has the function? If have ,how to do that? Thanks.
 
Posted: Thu Jul 14, 2005 6:02 pm    
 
As far as I am aware its not possible on any 08s or 12s, I think it may be available on some high end Coldfire devices.
Posted: Fri Jul 15, 2005 6:59 am 
 
Do you actually mean security rather than encryption? If so, see the flash blockguide for details. The security state of the microcontroller is governed by a byte stored in flash at address 0xFF0E.
Labels (1)
0 Kudos
Reply
0 Replies