How to add external ram in Processor Expert cpu build options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add external ram in Processor Expert cpu build options

1,793件の閲覧回数
AndersJ
Contributor IV
I want to add 256KB of external SRAM in normal expanded mode.
I am unable to add an external ram memory segment
using PE on the build options tab of the MC912SXD cpu bean.
* Name: RAM_External
* Qualifier: READ/WRITE
* Address: 140000 H
* Size 40000 H
 
At compile/link I get INTERNAL ERROR: at line 35 Unexpected status...... file: Drivers\HCS12\MC9S12_Linker.prg
 
Can anyone point out my error?
 
Thanks,
AJ
 
 
 
 
 
ラベル(1)
0 件の賞賛
返信
1 返信

755件の閲覧回数
ProcessorExpert
Senior Contributor III

This problem has been fixed in Processor Expert v2.99 for CodeWarrior v4.7. This version of Processor Expert is available as a service Pack on Freescale web.

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 件の賞賛
返信