How to Calculate Chip Temperature for 9s12vr?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Calculate Chip Temperature for 9s12vr?

1,420 Views
dli1
Contributor I

I wanted to read the chip temperature for a 9s12vr chip using its internal ADC channels.  I was able to read the ADC counts for the chip temperature and bandgap, but did not know how to convert it to temperature in degree C.  Unable to find the specification for the conversion.  Appreciate if anyone can post the conversion formula.

Labels (1)
0 Kudos
Reply
1 Reply

1,262 Views
RadekS
NXP Employee
NXP Employee

Hi David,

The temperature sensor has to be calibrated for giving enough accurate results. The offset and slope are specific for every MCU. The selected calibration method depends on required accuracy.

Please look at our application note AN3624 S12X Temperature Sensor

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3624.pdf

Some more general details about calibration may be found also in our application note AN3031 Temperature Sensor for the HCS08 Microcontroller Family

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3031.pdf


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply