How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)

2,772 次查看
Sully81
Contributor I
I am using Wytec's Dragon12 board to drive PWM for some 24V (5 Ohm, MAX 2 Amp) solenoids.  I am looking to spec out the transistor circuit to drive the coil but need to know how much current I can safely pull source from the MC9S12DP256 chip.  Can anyone point in the right direction to find this? 
标签 (1)
0 项奖励
回复
3 回复数

1,695 次查看
Sully81
Contributor I
Jim,
 
Thanks for the response.  It looks like the MAX source/sink current is +/-25mA.  Due to the relatively small source current, it looks like I'll have to use a darlington pair transistor to reach the high current needs of the solenoid.
 
thanks
0 项奖励
回复

1,695 次查看
bigmac
Specialist III
Hello,
 
Yes, you could use a darlington transistor, or alternatively a power MOSFET with a suitable maximum current rating, provided it is capable of fully switching with an input level of less than 5 volts.
 
For either method, if switching operation is infrequent relative to the switching time, dissipation should not be a major issue.  Both methods will also require suppression of inductive voltage surges.  The simplest method is to use a diode in parallel with the solenoid winding.  The diode should have a repetitive peak current rating equal or greater than the solenoid operating current.
 
If the MOSFET solution is used, a small series resistance in the gate circuit will limit the charging current into the gate-source capacitance, to be supplied by the MCU pin.
 
Regards,
Mac
 
0 项奖励
回复

1,695 次查看
JimDon
Senior Contributor III
Do you mean the MC9S12DP256 spec sheet?

You should have got a copy with the board.

Also, if you look on the schematic there should be a circuit that drives a relay, which you can copy except with a higher rated transistor.

0 项奖励
回复