How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How much current can I source to drive PWM using MC9S12DP256 (Dragon12 board from Wytec)

2,796件の閲覧回数
Sully81
Contributor I
I am using Wytec's Dragon12 board to drive PWM for some 24V (5 Ohm, MAX 2 Amp) solenoids.  I am looking to spec out the transistor circuit to drive the coil but need to know how much current I can safely pull source from the MC9S12DP256 chip.  Can anyone point in the right direction to find this? 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,719件の閲覧回数
Sully81
Contributor I
Jim,
 
Thanks for the response.  It looks like the MAX source/sink current is +/-25mA.  Due to the relatively small source current, it looks like I'll have to use a darlington pair transistor to reach the high current needs of the solenoid.
 
thanks
0 件の賞賛
返信

1,719件の閲覧回数
bigmac
Specialist III
Hello,
 
Yes, you could use a darlington transistor, or alternatively a power MOSFET with a suitable maximum current rating, provided it is capable of fully switching with an input level of less than 5 volts.
 
For either method, if switching operation is infrequent relative to the switching time, dissipation should not be a major issue.  Both methods will also require suppression of inductive voltage surges.  The simplest method is to use a diode in parallel with the solenoid winding.  The diode should have a repetitive peak current rating equal or greater than the solenoid operating current.
 
If the MOSFET solution is used, a small series resistance in the gate circuit will limit the charging current into the gate-source capacitance, to be supplied by the MCU pin.
 
Regards,
Mac
 
0 件の賞賛
返信

1,719件の閲覧回数
JimDon
Senior Contributor III
Do you mean the MC9S12DP256 spec sheet?

You should have got a copy with the board.

Also, if you look on the schematic there should be a circuit that drives a relay, which you can copy except with a higher rated transistor.

0 件の賞賛
返信