Hi Wave Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi Wave Problem

2,696 次查看
israel
Contributor I
Hello,
 
The Hi Wave gives me hard time. When stepping thorough a function while disabling the interrupt from the CCR the hi wave crashes many times every time in another line. is it a known problem or my code is bad?
I can not put my finger what exactly causes this problem. Can someone advise?
 
 
Roy
标签 (1)
0 项奖励
回复
2 回复数

1,558 次查看
Blackwolf
Contributor III
Hello Roy,
 
humm here some more details may be required:
_ does the problem occur on-board or in simulation ?
_ if on-board, which S12 is concerned and how are you communicating to the board ?
_ what do you mean exactly by 'hi-wave crashes' ? (windows exception ?hi-wave get frozen ? our application stands in an unstable state ?)
_ which HC(s)12(x) Codewarrior version is concerned ? (v3.1, v4.1, v4.5 ?)
 
As this issue may need some time to be investigated, I would suggest you to rather submit a ticket to the Technical Information Center, here is the link:
 
Send them the info above, if possible together with your project (in a zip file)
 
 
- BlackWolf -
0 项奖励
回复

1,558 次查看
imajeff
Contributor III
could be an unexpected interrupt request
0 项奖励
回复