Help - on motorola standard SGF Drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help - on motorola standard SGF Drivers

2,651 Views
lak
Contributor I
Hi,
I am using the motorola standard sgf flash drivers to erase/flash my MC9S12xDP512.
 
After running the NVMSectorErase(), I see that the page FD which I am trying to erase is partially erased. However the debugger when it loads, it erases the page completely but I can't.
I am running the code to erase, from RAM, so I feel I am not violating any of the restrictions of executing from the block to erase a page on the same one.
Even the NVMSectorErase() function returns no error, but not all locations are erased.
 
I downloaded these drivers under the MC9S12xDP512 product page of freescale website.
 
with regards,
Lak
Labels (1)
0 Kudos
Reply
4 Replies

1,242 Views
Alban
Senior Contributor II
Hi Lak,

It seems the SGF Flash drivers on S12X product page are for S12 and not S12X.
I don't know if anyone created a Service Request for this to be fixed.

Alban.
0 Kudos
Reply

1,242 Views
lak
Contributor I
Hi Alban,
I could get the S12X SGF drivers from the freescale support team. Luckily, these drivers are tested on the MC9S12xDP512 part and should possibly work for me.
 
with thanks,
Lak  
0 Kudos
Reply

1,242 Views
Alban
Senior Contributor II
Hi Lak,
 
That is very good news !
I asked the Documentation to modify the association for the right SGF drivers to appear on S12X products.
 
Thanks for putting the SR.
Alban.
0 Kudos
Reply

1,242 Views
lak
Contributor I
Hi Alban,
I have submitted a technical request for updated SGF drivers for MC9S12XDP512.
However, can you advice me whether there are any other specific flash drivers for S12X family?
 
with regards,
Lakshman
0 Kudos
Reply