HVI (ADC) input voltage range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HVI (ADC) input voltage range

ソリューションへジャンプ
1,617件の閲覧回数
aaronlee
Contributor V

Hi,

I have some question about HVI as follow:

How many input voltage range will be measure by ADC? 

  1. RatioL_HVI (2:1)
  2. RatioH_HVI (6:1)
  3. By pass divider

VHVI= -27 ~ +42V (in Table G-2. Absolute Maximum Ratings - High Voltage Input Pins - Port L)

What happen when i connect +15V to HVI pin with Ratio of 2:1, 6:1 or bypass?

0 件の賞賛
返信
1 解決策
1,367件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

 

The ADC input voltage must be in range of V_RL; V_RH.

An input level that exceeds this range will be clipped.

 

In case of HVI, the input voltage cannot reach the full scale of the ADC.

See absolute error on ADC (HVI Electrical Characteristics, Table G-1).

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,368件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

 

The ADC input voltage must be in range of V_RL; V_RH.

An input level that exceeds this range will be clipped.

 

In case of HVI, the input voltage cannot reach the full scale of the ADC.

See absolute error on ADC (HVI Electrical Characteristics, Table G-1).

 

Regards,

Daniel

0 件の賞賛
返信