HVI (ADC) input voltage range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HVI (ADC) input voltage range

Jump to solution
1,590 Views
aaronlee
Contributor V

Hi,

I have some question about HVI as follow:

How many input voltage range will be measure by ADC? 

  1. RatioL_HVI (2:1)
  2. RatioH_HVI (6:1)
  3. By pass divider

VHVI= -27 ~ +42V (in Table G-2. Absolute Maximum Ratings - High Voltage Input Pins - Port L)

What happen when i connect +15V to HVI pin with Ratio of 2:1, 6:1 or bypass?

0 Kudos
Reply
1 Solution
1,340 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

 

The ADC input voltage must be in range of V_RL; V_RH.

An input level that exceeds this range will be clipped.

 

In case of HVI, the input voltage cannot reach the full scale of the ADC.

See absolute error on ADC (HVI Electrical Characteristics, Table G-1).

 

Regards,

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
1,341 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

 

The ADC input voltage must be in range of V_RL; V_RH.

An input level that exceeds this range will be clipped.

 

In case of HVI, the input voltage cannot reach the full scale of the ADC.

See absolute error on ADC (HVI Electrical Characteristics, Table G-1).

 

Regards,

Daniel

0 Kudos
Reply