HCS12 development board query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12 development board query

1,960 Views
Sinky
Contributor I
I have been doing work with the SCI of the HCS12 on a MCU PROJECT BOARD -2 but since i only have access to one of these i wanted to use PBMCUSLK's. The PBMCUSLK boards which look pretty much the same as the MCU PROJECT BOARD -2 but when i run my code on it, it says illegal_bp in the command window of the debugger.
 
I have checked the jumpers and they are the same on both. Is there a difference between both of these development boards? Does anyone know what the error means or how i fix it?
 
Thanks
 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,115 Views
Xbot
Contributor II
I  believe there is no SCI module connected to this board. testing is futile.
0 Kudos
Reply