HCS12 In-Application Reprogramming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12 In-Application Reprogramming

3,464 Views
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Sun Apr 17, 2005 1:31 am    
 
Hello,

I want to develop an application for HCS12E128 and introduce the possibility of updating the software application through RS232, without any external hardware, the command for reprogramming will be with a RS232 command to initiate the process. Any idea how to organize the loader, application, interrupt vectors update,...?
Someone have experience in this?

Regards,
 
Posted: Mon Apr 18, 2005 9:58 am    
 
There's a RAM bootloader for the S12 in AN2546 that uses the CAN and SCI ports. This loads what you need into RAM.
You may be able to take this as a starting point and modify it for your individual needs. In general you want to avoid having the flash programming algorithm stored in the part.

Other useful documents are: AN2720 and AN2548
 
Posted: Tue Apr 19, 2005 12:18 pm    
 
a thought - run a fixed boot loader out of an unpaged area and set a flag in e2 when its time to upgrade. reboot the device and in the boot loader check if its time to upgrade. start up SCI and bring down the new file. when ur done with the writing the code down to the device clear the flag in e2 and reboot again and jump to your new program.
Posted: Mon Apr 25, 2005 7:11 am  
 
There is an app. note. AN2720/D that might help you.
Labels (1)
0 Kudos
Reply
0 Replies