HCS12. Address space of external devices in expanded wide mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS12. Address space of external devices in expanded wide mode?

2,944件の閲覧回数
Trace
Contributor I
Hi,

After reading the app note on accessing external devices, another thing that troubles me is the address space when using expanded wide mode. For me it looks like that when using the expanded wide mode all addresses from 0x4000 to 0xFFFF is taken from outside? Including the vector area? Is this really true?

I only need to attach a 16bit wide DAC to my design… so I only need a very small address space for that. 4 – 16bit addresses actually. Is it possible for me to place that on the bus and still be able to use all the internal flash including the vector space?

Would it be better and just as fast if I just emulated an addr/data bus on some ports instead?

Thanks in advance!

Best regards
Jan Thogersen

Message Edited by Trace on 03-14-200606:08 PM

ラベル(1)
0 件の賞賛
返信
1 返信

802件の閲覧回数
Steve
NXP Employee
NXP Employee
Jan, have a look at http://www.freescale.com/files/microcontrollers/doc/app_note/AN2287.pdf. The first 13 pages describe the concepts behind the external bus on the S12 and then it goes on to provide hardware connections.
Basically you have a choice of whether the internal Flash is available or not in expanded mode (see the ROMON and ROMCTL descriptions in your datasheet). Depending on the S12 in use you may have a choice of where the ATD can go in the memory map. Devices with small internal memories have more flexibility with this.
Start with the app note and let us know if you have any more questions.
0 件の賞賛
返信