HCS 12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS 12

4,656件の閲覧回数
eagle
Contributor I

Bonjour Fabrice,

 

 Hi all,

 

 

I wanna make a HCS12 board:

 

but i don't know if  :  this board ( http://www.allactivex.com/programming/hcs18u3o.htm) + BDM (P&E’s USB HCS08/HCS12 MULTILINK)(http://www.pemicro.com/index.cfm?targetURL=http://www.pemicro.com/products/products_find.cfm) + CodeWarrior (Special Edition Evaluation) = are compatible,

 

 

Can i star with this kind of equipement !!!!

 

thx

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,045件の閲覧回数
eagle
Contributor I
Mike  if u have any adress where i can have a small board with a minimal support, send them to me .. ....
 
thx
0 件の賞賛
返信

2,045件の閲覧回数
eagle
Contributor I

thx Mike,

yes i am out the us, exactlu europ ....

i don't know why !, but i haven't understood very well ....

my qustion was if the three compoments are compatible (so i can develop without problem), or i have to change some one of them (i am new in this field)

 

and thx again mike

 

 

0 件の賞賛
返信

2,045件の閲覧回数
mke_et
Contributor IV
Well, I'd have to ask why they made the BDM 'custom' to the board and not the 6-pin header the BDM pods (the USB BDM Multilink for example) generally come with. I didn't look that close, but whenever I see something like that, I assume there's an engineer with 'the clevers' out there and if there's other issues down the road, guess who will be stuck solving them?

But, and I didn't do more than glance at it, if it works with the BDM, even if you have to make a custom pin translation adapter, go for it.

However, I would think it might be easier to find one the 9S12Badge boards that are floating around. I've used them to do a LOT of my prototyping, and even some complete projects. Same kind of idea, a small board with CPU and minimal support, like power and one serial line, and pins to tie to anything you want. I think at most they went for $62 when new. (I got my first ones for $12 by attending a 'Future' seminal and getting a $50 coupon to make it come out to '12' dollars.) They've been discontinued for a while, but they're still out there. I needed a couple more last fall and my Future rep found them for me in a couple of hours. They were used, but they worked fine.

Mike

Just noticed, are you out of the US? I see the board you're refering to is non-US. If that's an issue, then that's also something to consider...

Message Edited by mke_et on 2006-06-20 09:13 AM

0 件の賞賛
返信