FreeRTOS & TCP/IP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS & TCP/IP

3,601件の閲覧回数
RChapman
Contributor I
This message contains an entire topic ported from a separate forum. The original message and all replies are in this single message. We have seeded this new forum with selected information that we expect will be of value to you as you search for answers to your questions.
 
Posted: Sat Jun 18, 2005 9:20 am    
 
Hi Guys
I starting to look into a project where I would like to use the MC9S12C32 running the FreeRTOS and TCP/IP. the idea is to read some sensors and send the info using TCP/IP. the question is: is this practical interms of instructions overhead.
All thoughts welcomed.
best regards
 
Posted: Sat Jun 18, 2005 2:32 pm    
 
I believe the NE64 may be a better chip for this type of project as it has ethernet support built in.

http://www.cmx.com/freescale/
http://www.cmx.com/

Hmm my wife is nagging me to get off her laptop ill be back in a bit just google NE64
Posted: Mon Jun 20, 2005 7:44 am    
 
Hi
Is definitely a nice chip, but I already have the C32 eval board and also the E128 eval board so I would like to used them if possible.
This is just a sort of investigation on how to use the TCP/IP stack and a real time OS, maybe later it will become something more, but at the moment I do not want to spend to much money on it.
thanks for your help, the NE64 is very interesting and the CMX RTOS is very nice.
best regards

Posted: Mon Jun 20, 2005 12:20 pm    

http://www.freescale.com/files/microcontrollers/doc/app_note/AN2304.pdf

may be a good place to start. They are talking about a UDP/IP implementation though, which can still get data across the net and is easier to implement in some situations. Have you tried googling for much info?

Posted: Mon Jun 20, 2005 12:26 pm    

Should you want to purchase an NE64 at some point this may be a good option and may swap out with one of your existing EVB's depending on who they are from.


http://www.technologicalarts.ca/catalog/index.php/cPath/50_69

Posted: Tue Jun 21, 2005 7:10 am    

Thanks,
that is a very nice product and even nicer price...
the Freescale board is about $240, so you can not go wrong.
I will probably buy one of this I think, just have to disguise it on my next order...
Have you used this board your self?
Thank you for your help
regards

Posted: Tue Jun 21, 2005 11:03 am    

 

Quote:
Thanks,
that is a very nice product and even nicer price...
the Freescale board is about $240, so you can not go wrong.
I will probably buy one of this I think, just have to disguise it on my next order...
Have you used this board your self?
Thank you for your help
regards


No, I have not used that board. Remember though that is a module meant to plug into one of there other boards. You might want to give them a call/shoot them an email to figure out what is the best way for you to get setup. My C32 demo board was a free gift from Future Electronics which is a module and the parent board. I think there parent boards are designed so any of the modules can swap in/out with each other. I have not looked into it too much but they are not a bad place to get eval boards. I have never used the Wytec boards http://www.evbplus.com/ but they seem to be priced reasonably too. For beginners they have quite a few options on them at a reasonable price! I don't know that they offer anything for the NE64 though. Anyhow I gotta run I am about to be late for work! Smile


ラベル(1)
0 件の賞賛
返信
0 返答(返信)